NXP Lighting News - June 2012
Latest NXP News in Lighting Technology
Subscribe, NXP Lighting News 2012
Contents:New ProductsApplication SpotlightNXP in the News
NEW LITERATURE / APPLICATION NOTES

AN11136: Buck converter driver for SSL applications
CLICK HERE >

AN10962 Dimmable CFL using the UBA2026X family
CLICK HERE >

EVENTS!

6th European ZigBee Developers' Conference
June 27 - 28, 2012
Munich, Germany
June 28: NXP is presenting the "Wireless Control Systems for Smart Lighting" session
CLICK HERE >

Strategies in Light Europe
September 18-20, 2012
Munich, Germany
NXP will be presenting on wired and wireless smart lighting
CLICK HERE >

RESOURCES

New Products

SSL21101 NXP non-dimmable flyback driver for LED lighting SSL21101

This flexible, one-stage solution enables a small design with a low bill of materials. It offers very high efficiency, uses special operating modes to increase performance, and is equipped with a complete set of protections.
LEARN MORE >


Application Spotlight

JenNet IP Beyond Smart Lighting

Internet-enabled Smart Lighting signals a fundamental shift in how we interact with lights – helping individuals, businesses and governments save energy. This video, partly filmed in a San Jose, California home with a 70-node smart lighting network, explores the universe of possibilities enabled in a world where every light bulb has an IP address.

NXP solutions featured include the GreenChip smart lighting solution (GreenChip iSSL and iCFL), which incorporates JenNet-IP network layer software. Based on 6LoWPAN, JenNet-IP enables ultra-low-power wireless connectivity and can be extended to other smart devices in both residential and commercial buildings.


Reference Design Boards

JenNet IP Beyond Smart Lighting

SSL21101 230V
8W Flyback retrofit SSL lamp reference design – Low THD CLICK HERE >

SSL21101 120V
8W Flyback retrofit SSL lamp reference design – Low Ripple CLICK HERE >

SSL21101 120V
8W Flyback retrofit SSL lamp reference design – Low THD CLICK HERE >

SSL21101230V
8W Flyback retrofit SSL lamp reference design – Low Ripple CLICK HERE >


NXP in the News

What's Next for Internet-Enabled Smart Lighting?

Eindhoven, Netherlands, May 8, 2012 – What if every light bulb had an Internet IP address? Since NXP Semiconductors N.V. (NASDAQ: NXPI) first raised the question at LIGHTFAIR International (LFI) nearly one year ago, interest in IPv6-enabled smart lighting has soared. The potential energy and cost savings – as well as the comfort, convenience and lifestyle benefits for the consumer – have mobilized a growing ecosystem of innovators in lighting, connectivity, energy management and home automation to enable and support wirelessly controlled intelligent lighting. READ MORE > GreenChip Smart Lighting Remote Control