subscribe
Contents: New Products, In the News, Application News, Educational Tools New Literature: Application Note New Literature: Leaflet Events

New Products

The best reception of GNSS signals with
the smallest footprint

SiGe:C GPS LNAs BGU700x/BGU8007
By dynamically suppressing strong cellular and WLAN transmit signals, an industry first, these LNAs offer the best reception of weak GPS signals. Linearity improves with a 10 dB better IP3 under -40 to -20 dBm jamming conditions, while NF remains below 1 dB. Requiring only two external components, they save up to 50% in PCB size and 10% in component cost, offering the smallest footprint in the market.

> READ MORE

tff101

In the News

Dow Energy Dissertation
prize for NXP Employee, Edmund Neo

Edmund Neo, Principal Application Engineer at NXP Semiconductors Nijmegan

On November 10, 2011, Edmund Neo, Principal Application Engineer at NXP Semiconductors Nijmegen, received the Dow Energy Dissertation Prize from the Minister of Economic Affairs for his innovative doctoral research "Highly Efficient and Highly Linear RF Power Amplifier", bringing efficiency improvement for Base Stations Amplifiers, reducing the CO2 emission, and saving cost for the network providers.

> READ MORE

The Excellent Core Partner Award

On November 3, 2011, NXP Semiconductors received the prestigious Golden Award as Huawei’s Excellent Core Partner at Huawei’s corporate headquarters in Shenzen, China. NXP’s innovative solutions and continuous dedication has resulted the recognition from Huawei for 3 years in a row.

> READ MORE


Application News

Multi-standard MIMO radio base station transmitters

The spatial multiplexing scheme used to implement MIMO relies on the ADC receiver data streams and the DAC transmitter data streams being sample synchronous and phase coherent. Maintaining sample synchronization is typically accomplished using brute force methods – FPGA-based state machines plus complex data converter clock and reset logic at board level. New data converters now embed multiple device synchronization functionality, making the implementation of MIMO transceivers much easier than with older obsolete high-speed converters without this functionality.

This white paper presents brief overview of the challenges associated with MIMO transceiver design and a simplified theory of operation for NXP Semiconductors CGVxpress MDS feature.

> LEARN MORE

Educational Tools:

Videos

NXP GPS and FM Low Noise Amplifiers: Best Reception at Smallest Footprint

video

Resources:

Design Tool Portal

NXPs online design portal helps simplify your design with free online tools

> Click here

Cross Reference Tool

The new cross-reference tool is primed with several thousand competitor part numbers

> Click here

Quick Links:

Sample Kit

Sample Kit

Available Now! Sample kit for QUBiC4 Si and SiGe:C transistors for any RF function (BFU6x0 &BFU7x0).

This sample kit contains a selection of RF transistors based on NXP’s new 6th & 7th generation. Use the selection guides (on the sample kit) to select your preferred type. New 6th & 7th generation RF transistors from NXP offer the best RF noise figure versus gain performance, drawing the lowest current. This performance allows for better signal reception at low power and enables RF receivers to operate more robustly in noisy environments. Available via your authorized NXP distributor or local NXP representative.

> Click here




About NXP Semiconductors

NXP Semiconductors N.V. (NASDAQ: NXPI) provides High Performance Mixed Signal and Standard Product solutions that leverage its leading RF, Analog, Power Management, Interface, Security and Digital Processing expertise. These innovations are used in a wide range of automotive, identification, wireless infrastructure, lighting, industrial, mobile, consumer and computing applications. A global semiconductor company with operations in more than 25 countries, NXP posted revenue of $4.4 billion in 2010. For more information visit www.nxp.com
SUBSCRIPTION INFORMATION: For new registrations go to:
http://www.nxp.com/campaigns/high-performance-rf/newsletters
NXP | Privacy policy | Terms of use
NXP Semiconductors | High Tech Campus 60, 5656 AG Eindhoven, The Netherlands | 2006-2009 NXP Semiconductors. All rights reserved.